This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LEDMCUEVM-132: Programming this EVM

Part Number: LEDMCUEVM-132
Other Parts Discussed in Thread: MSP432E401Y

Tool/software:

Hi,

I would like to integrate this EVM with an external ADC through SPI. Do I require any external debuggers to program this? Could I connect this to the CC Studio, and try my programs? 

Thanks

Ram.

  • This EVM is essentially the MSP432E401Y EVM without the debugger and a bunch of other devices to facilitate communications for our LED drivers using either SPI or UART over CAN.  You can use the JTAG connector to program it.  

    -fhoude