Other Parts Discussed in Thread: , TPS25751, BQ76905
Tool/software:
Hello,
I am looking to build a battery management circuit using Lifepo4 2S3P INR26700 cells topology.
With a nominal battery voltage of 3.2V and 4.5Ah, these cells should give me approx. 86.4Wh and working with 6.4V it is exactly what I need for my application.
The charging voltage is a 7.3V max and 6.75A max for current. I would like to use a USB Type-C PD interface.
Can you please recommend an IC(s) and a BMS charging circuit? (ie. USB controller, charge controller, protection)
Thanks,
-Tal