Other Parts Discussed in Thread: SN62826,
Tool/software:
Hi,
For SN62826/7, does it is force PWM mode or PSM/PWM mode?
If we need quick output discharge, we need choose B version, right? May I know the output discharge resistor value?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
Thank you for using E2E,
For SN62826/7, does it is force PWM mode or PSM/PWM mode?
It's PSM/PWM mode device.
If we need quick output discharge, we need choose B version, right?
The discharge current is same as TPS62826.
In SN62826, VIN must remain present and within the recommended operating range for the discharge to function. In SN62826B, the active output discharge can function as long as the VIN is above 2.0 V.
Another question, for datasheet C3, what is the capacitor range? Can I use 150pF?
For the recommended 100k value for R2, a 120pF feedforward capacitor is used. C3 = 12μ/ R2.
Can you contact me via email: m-shaik@ti.com
Thank you & regards,
Moheddin.