Tool/software:
Hi,
I am wondering why the low-frequency (0.01kHz to <1kHz) PSRR varies a lot for different load currents, e.g., in Figure 5-20, PSRR@0.01kHz varies from ~-70dB for 20mA load to ~-50dB for 250mA. From what I understand, the PSRR in low frequency region is dominated by the Bandgap PSRR, which should not vary across different load currents.