Other Parts Discussed in Thread: TPS3808E
Tool/software:
The TPS3803-01DCKR is characterized by the following parameter: Input clamp current, IIK (VI < 0 or VI > VDD) = ±10 mA.
But if I measure the existence of a diode between the SENSE and the VDD pins (i.e.: pins 5 and 4 respectively) I don't detect any diode.
I used the "Diode" function of a Fluke 179 multimeter, and I tried both the polarities: positive on SENSE and negative on VDD and positive on VDD and negative on SENSE. In both cases the multimeter showed "OL", taht is the indication showed when the tips are not connected at all.
I'd like to know the mechanism allowing this device to clamp the injected current.
Thank you in advance,