Hello,
Can PWRON pin be connected directly to VBAT pin without using a pull-up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would recommend connecting a resistor to control the input current on this pin.
Does it matter if it is Master or Slave mode? The VBAT supply is generated by USB. And I believe there is already a current limiting function. So the resistor may not be needed.
Also does 32KHz clock or IO.1P8 to be present before PWRON goes high?
We have the 32KHz clock driven by an oscillator and the one change we made that caused the TPS65930 to consistently power-up in slave mode was to have the 32KHz clock present when PWRON was applied. If the 32KHz oscillator is powered by VIO the device never powered up. Is the PWRON input sampled by the 32KHz clock? Since slave mode requires a 32KHz oscillator and a crystal cannot be used, what power rail should it be driven from? Are there any power boundary issues to be concerned about?
The TPS65950 on the BeagleBoard powers-up in master mode and uses a 32K crystal. Since our design uses a 32K oscillator and not a crystal does this clock need to be present to power-up successfully in master mode also?
What exactly is the voltage supplied to IO.1P8 used for inside the device?
I didnt understand your comment about pull-up resistor. You provide power from any source it is recommended that you have a resistor on this supply.
For slave mode 32K clock has to be available before powering the device. Internal clock is bypassed in this mode. Supplying the 32K clock with VIO will not help (chicken and egg). You will have to find another source available on your platform.
IO is always 1.8V on this device.
Some additional questions:
1) Since the 32KHz clock is required to power-up in slave mode and IO.1P8 should be connected to VIO per a previous email, am I correct in assuming that it is OK to drive the 32KHz clock input from an oscillator without power present at the IO.1P8 pin?
2) If we use an external 32KHz oscillator (not a crystal) and power-up in master mode, does the 32KHz clock need to be present for the TPS65930 to power-up?
3) Am I correct in assuming PWRON can be tied to the VBAT.USB rail (3.6V) in both master and slave modes?
1. Yes, IO.1P8 will be powered up when VIO is ON. IO.1P8 has to be connected to 1.8V. I will confirm if 1.8V from PMICs VIO is ok or not.
2. 32K is always required for power-up irrespective of the mode.
3. To answer this question I would request that you provide some details about your system in terms of a block diagram. Generally the device and the whole system is powered by a single battery. All power comes from a single source(battery). I am unable to understand what you mean that the supply will come from VBAT.USB, isnt there a common battery for the system?
Also, in slave mode PWRON is used to power ON and OFF the system. Do you plan to use PWRON for such a function?