Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74701-Q1: Does it pass ISO7637-2 pulse5a?

Part Number: LM74701-Q1

Tool/software:

Hi team, 

We are interested in TVS less solution. In the datasheet, It passes ISO 16750 Pulse 5B but it looks 35V suppressed load dump. There are two questios shown below.

  1. ISO16750-2 pulse 5a/5b are corresponding to ISO7632-2 pulse 5a/5b respectively?
  2. Is this device suitable for ISO7632-2 pulse 5a (unsppressed load dump)? Or to pass that, do we need 35V suppressor TVS externally?

Regards,
Ochi