This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74900Q1EVM: Modifying EVM to push 30A through board

Expert 3801 points
Part Number: LM74900Q1EVM
Other Parts Discussed in Thread: LM74900

Tool/software:

Hi Team, 

I'm working with an engineer that would be interested in pushing 30A through the LM74900, but would like to test it first using the EVM. On our EVM, we note that you can only pass 10A max current through the current setup, so I wanted to understand if the 10A Max current is due to the components (MOSFET, Rsense, other passives, PCB traces, etc...), or if this board can be modified to pass 30A of current?

Anything more than 10A would help, so any guidance or feedback here is appreciated. 

Thanks,

JP