This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: AON6226 Alternative

Part Number: BQ25750

Tool/software:

Hello,

I am currently working on a design using the BQ25750. The EVM FET is a AON6226.

The Input voltage MAX will be 15Vdc and I am only charging a 4S LiFePO4 pack at 500mA.

I would like to use a smaller (cheaper) FET option, but I am unsure where to start, since all of the examples are for much higher current.

Do you have any recommendations?