Other Parts Discussed in Thread: CSD95510, CSD95560
Tool/software:
Hi Team,
I am getting fault in STATUS_MFR_SPECIFIC (80h) command bit 4 and 6 is asserted.
Also there is fault in STATUS_OTHER command bit 0. And in Status EXTENDED(0XD0) bit 25.

Even after Clear faults is done in Status tab, only bit 0 in STATUS_OTHER (FIRST_TO_ALERT) is getting cleared.
Then using CLR in STATUS_MFR_SPECIFIC and STATUS EXTENDED all faults are cleared. But did not get the required Vout (it is set to 1.1V).
Getting Vout as zero, as attached in image below.

Again when Clear Faults is done, getting fault only for PH_ERR(bit 4 in STATUS_MFR_SPECIFIC) and Vout as 0.002V.
Can you tell why this error is there and why I am not getting required Vout.
Regards,
Siddhi
to gain access to this tab.