Other Parts Discussed in Thread: BQ25792, TPS25751, TPS54531
Tool/software:
Do I need a PP5V input to the TPS25750D (applcation with BQ25792)? In the user giude "slvubz4_TPS25750_userguide.pdf" there is a solution shown w/o such input (page 3, right side of fig. 2-1) also for sink and source application. In other documents a 5V/5A supply for PP5V is used. Why can the BQ25792 not generate this voltage for the USB output (VBUS)? Or is the 5V needed for the TSP25750 internally?
Best regards