Other Parts Discussed in Thread: BQ24725
Tool/software:
Hello,
I'm intending to use the BQ24725a charger in my design for charging in up to 9A charging current and voltage 12.5v.
According to the Typical Application and also according to the EVM scheme the Cout is up to 30uF not more. It is written there that it was planned for charging in about 3A-4A.
My question is what shall be the charger output capacitance (C-out) on the phase pin after the inductor in case of charging in about 9A-10A?
From what I'm familiar with, usually the output capacitance of buck converter when output current is 9A-10A is around 300uF so 30uF and even 60uF looks surprising to me.
Could you also send a tool for calculating the charger output capacitance dependent the output current/voltage ?
Thanks,
Ohad