Other Parts Discussed in Thread: TL431, TLV431, UC3844
Tool/software:
Hi team,
When customer want to use UCC28C42 in the new circuit design. Vin=19.2VDC. There are total 3 outputs. Vout1=5V 0.7A(main feedback winding). Vout2=+15V 0.55A Vout3=-15V 0.3A.
When only add load on Vout1=5V 0.7A, the circuit seems to be unstable with loop Oscillation.

CH1:CS pin CH2: OUT CH3:COMP CH4:pin1 for opto-coupler HPC1018.
The primary inductor is 40uH.CTR of optocoupler is 130-260%.

Can you help check what might cause the issue? This is new opportunity for us to gain business in new area. Looking forward to your reply!