Tool/software:
The picture below shows the design I have made. When i supply the input with 24 VDC (current limit set to 1 A) my current limiter is triggered and the voltage drops to ~1V. So the regulator never starts. Is there any obvious mistakes that could cause this problem? I have checked the circuit, and there are no short circuits or components placed in the wrong way. I have isolated this circuit so there is no load attached when I turn on the input voltage.