This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS75003: New gen of TPS75003RHLTG4

Part Number: TPS75003
Other Parts Discussed in Thread: TMS320VC33

Tool/software:

Hi team,

Is there any recommendation for a PMIC with performance close to TPS75003RHLTG4?
Briefly describe the current PMIC usage scenario;
3-way output Vo1=3.3V; Vo2=1.8V; Vo3=1.2V
Vo1 & Vo2 provide DSP (TMS320VC33) DVDD=3.3; CVDD=1.8; —— Peripheral device SRAM 4PCS = 3.3
Vo1 & Vo3 provide FPGA (LFMXO5-25-8BBG400I) —— Peripheral device SRAM 4pcs + Flash + eprom = 3.3

Thanks

Lillian

  • Hi Lilian,

    Based on your information and depending on the load requirements and how much current is needed, we have the LP87563 or the LP87523. These should be able to reach your desired output levels of 3.3V, 1.8V, and 1.2V.

    Thanks,
    Field