This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: Design recommendation

Part Number: LM74700-Q1

Tool/software:

Hi,

We are using LM74700QDBVRQ1- Automotive ideal diode controller. and IPB120N06S4 ( Infineon N-MOSFET) is used as controller mosfet which has VGS(th) = 4V(max).

Please provide us a confirmation whether this Mosfet is good to use ( since it has higher VGS(th) we are confused ). If not please suggest a MOSFET.

Max Load current = 8A 

Min Input Voltage = 9V

Thanks in advance!!!