This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156: Schematic check request

Part Number: LM5156

Tool/software:

Hi Sir,

we specifition is INPUT12-60V, OUTPUT 12V/6A.

may we know this schematic is ok? if there suggestion or need modify please let we know and learn from you, thanks.

ISOLATED_DC_INPUT_LM5156 - 編輯PDF.pdf

AE-SFD25005_A.pdf

  • Hi Tommy, thanks for using E2E.

    I checked the schematic and it seems to be ok. Maybe the loop compensation has to be adjusted once the design is built.

    Two points i found:

    1. I would recommend to add a PNP transistor to the primary side softstart like in below picture. This will limit the duty cycle also in the first switching cycles.

    2. In your design you supply VCC externally with an AUX winding. The transistor of the optocoupler is pulled up to this voltage. In case of voltage variations, the regulation can be affected. To avoid this, a zener diode can be used to clamp the pullup voltage to a certain level:

    Best regards,

    Moritz

  • Hi Moritz,

    got it, thank for you support, has been modify schematic as below.

    ISOLATED_DC_INPUT_Circuit_LM5156_20240605.pdf

  • Hi Tommy,

    Yes, now it looks good to me.

    Best regards,

    Moritz