This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B:able to use with any WPC charger

Part Number: BQ51050B

Tool/software:

BQ51050BEVM-764を用いたワイヤレス充電受信回路を設計しています。
市販のQi準拠の送信機を使用する予定です。
しかし、このフォーラムで「標準のWPCトランスミッターでは動作しません」というメッセージを見つけました。(cb narayana 2023年11月3日)私も同様のアプリケーションを使用するつもりです。
BQ51050BEVM-764を用いたワイヤレス充電受信回路を設計しています。「BQ51050B AmazonのどのWPC充電器でも使用できます」を教えていただけますか?%MCEPASTEBIN%(パーセント・マケペースト・ビン)

  • Hello

    Translation of above:

    I am designing a wireless charging receiver circuit using the BQ51050BEVM-764.
    I plan to use a commercially available Qi-compliant transmitter.
    But I found the message "does not work with standard WPC transmitters" on this forum. (CB narayana November 3 2023 ) I intend to use a similar application.
    I am designing a wireless charging receiver circuit using the BQ51050BEVM-764. Can you tell me "BQ51050B can be used with any Amazon WPC charger"? %MCEPASTEBIN%

    Ref Post by CB Narayana--see here

    Bill J -- The BQ51050B is designed to Qi standard and will work with Wireless Power Transmitters also designed to the standard.

    "Can you tell me "BQ51050B can be used with any Amazon WPC charger"? " --- Bill J -- If the Transmitter is designed to standard and Certified to Standard it should work.