Other Parts Discussed in Thread: EV2400, BQSTUDIO
Tool/software:
Hi team,
I have a 64 cell lion battery pack. I am using BQ34Z100 to measure pack parameters. I have tested the same golden image file with the EV2400 EVM board for 48V, as well as on my own PCB. The golden image does not remain restored on our PCB when the power is cycled, but remains intact on the EVM even after power cycling the fuel gauge.
Basically, once I prepare an image file on one gauge, after a power cycle or on a new fuel gauge, I have to reflash the image and re-calibrate everything from scratch.
Kindly let me know if there are certain hardware design changes from the EVM design schematics, which need to be done for multi-cell applications.
I have been using this design as reference. -
Regards,
Shreya