Other Parts Discussed in Thread: LMG1020
Tool/software:
I'm using this board to activate a 5W diode laser, but it's not working. After checking the test points i notice that In+ value is always 0, like if isn't working. After checking the datasheet of that component (SN74LVC1G08DCKR), it's a simple AND, that it's connected to one of the sources of the board(J3). I'm asking if there's any test i can do to see if the component is broken and what's the need of this component, because both inputs are connected to the same source, so they will always be the same value in my opinion. Thanks.
Best regards,
Marcos Madureira