This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145-Q1: LM5145QRGYRQ1

Part Number: LM5145-Q1
Other Parts Discussed in Thread: LM5146

Tool/software:

I have design buck converter (LM5145-Q1), input voltage is 54V and output voltage is vary from 1V to 10V by adjusting feedback resistor at max.8A load. I am getting expected output voltage as per feedback resistor adjustment without load. The moment connect load at min.0.5A load, then output voltage is dropping too much square ware is coming at output. Please find the circuit diagram below