This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22811: Maximum Load Current

Part Number: TPS22811


Tool/software:

I was wondering if I could use this load switch at 10A? Would this destroy the device or reduce its useful life?

Thanks

  • Hi Curtis,

    Yes, the device can support maximum 10A current. If you ensure that the junction temperature is within 125C during steady state operation, then the device life won't be affected. 

    (Basically, as long as the operating conditions are within the recommended operating conditions, the reliability and functionality are maintained, between recommended and absolute, all functionalities cannot be guaranteed, beyond absolute max, device will get damaged)

    You can also calculate FIT rate using this: https://www.ti.com/lit/an/spraby3/spraby3.pdf 

    Click resolved if this answers your question. 

    Best Regards,
    Arush