Tool/software:
Dear TI engineer.
I'm using 3000mAh Li-ion battery with 4S4P connection.
Therefore in my application, 1C charging current is 12A.
My question is that, can I 12A charging with BQ24600 IC?
Refer to datasheet, "VIREG_CHG = VSRP – VSRN = 100mV" with +-3% accuracy.
I think that if I use 8.3mΩ sensing resistor, I can set the 12A of charging current.
Maybe charging current accuracy will be reduced. If charging current accuracy is not reduced dramatically, I can take it.
And I want to know whether there is abnormal current oscillating or ripple occur or not.
Thankyou for your interest.