Other Parts Discussed in Thread: BQ25798
Tool/software:
Hi Team,
1. I want to know the POR definition of the BQ25792. If battery is connected, but re-plug in VBUS, does this action mean POR?
2. Currently, we have Vbus and battery connecting the BQ25792. Now we re-plug in the Vbus and we don't want the 1h/3h/5h/6h the register setting changed. Do we have any bit can achieve the function?
3. For the CC/CV threshold, it's regulation voltage that we set, but I'm not sure if we can set VREG_low threshold which means that if the battery discharge the voltage and its value low than VREG_low threshold and then enter in CC mode to charge, but the VREG_low threshold isn't the same as VREG.

Regards,
Roy