Other Parts Discussed in Thread: TLV773
Tool/software:
Hello team,
My customer is looking for an LDO with strict area requirements. Does TI have an LDO that can meet the following requirements? Could you introduce me to an LDO that meets the requirements as much as possible?
For example, does TLV772 meet their size requirements of 3mm x 3mm (including peripheral components) ?
Customer’s Requirements
Input Voltage: 5V
Output Voltage 3.3V
Output current: 100mA or more
Mounting area: Approximately 3mm x 3mm (including peripheral components)
Heat: Ambient temperature +30℃ or less
Thank you for your help.
Regards,
Taito Takemura