This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55332-Q1: Design procedure example and confirmation tool

Part Number: TPS55332-Q1
Other Parts Discussed in Thread: LM5158, LM5157

Tool/software:

Hi,I want to use the TPS55332 in a new design and to do so, I'm trying to understand the example implementation in the section 8.2.1 (datasheet) and I can't understand where some values come from, especially in the output capacitor selection (8.2.2.1).
For example, using the equation 19 the output capacitor value is 0.37uF, I replace the design parameters according to table 1 (datasheet) and I can't get the same result.

I use:

Vin = 14V

Vo = 25.5V

fsw = 2MHz

Io(max) = 0.3A

▲Vo = 0.52

Then, C > 0.13 uF

On the other hand, in equation 26, what are Itran and Vodrop?

Finally, is there a tool that I can use to verify or validate my design in the future?

I'm sorry if the question is so silly.

Best regards,

Christian