This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Bq78350-R2 unit of Battery Low % parameter

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

Hi everyone,

SLUUBD3E(9.1.5) says Battery low unit is 0.01% , so the default value for 7% is 700. But I checked and saw 7.00 not 700, which one is correct? What should I write in the registry to make it 5%? 500 or 5?