Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hello,
I have a problem with a new designed PCB in single cell configuration. The cell inputs VC1-VC4 are connected together. On the cell and on the output side a stable voltage is applied. The communication to Battery Management Studio 1.3.125 works, but the device does a continious restart event. Unfortunately it is not possible to change DA configuration or write SREC or GG file, so I expect device recognizes a permanent fail because of cell voltage low.
How is the procedure to initially configurate as 1-cell application device? Which steps can we do to prevent shutdown, before setting the right cell configuration?
Thanks
Torsten