Part Number: TPS92663A-Q1
Tool/software:
Hello,
I have a Question related TPS92663 and TPS92662 to be in the same ,and for Example I want to write Broadcast frame to write the M Phase Registers for Both and I will use 16 byte Write
so for TPS92662 it will be ok ,but for TPS92663 what could be the behavior ?
1. It will reject the frame .
2. it will receive the frame and it will write the data in addresses sequentially without over writing the M width as there's a gap between them and LSB data (8-bytes) would be written .
3. it will Receive the frame and it will write the data an it will over write the M-width bytes.
Best Regards,
shaher