Part Number: TPSF12C1
Tool/software:
Hi,
Q1
The datasheet states "Withstands surge of 6 kV (IEC 61000-4-5) with minimal external component count." Is there any reference information for obtaining IEC 61000-4-5? Examples of demonstration experiments such as lightning tests/impulse tests and circuit configurations.
Q2.
Can you explain in detail the mechanism by which the coil becomes smaller using AEF?
Q3.
I'm worried that external noise will damage the IC. Is there any information on external noise immunity?
Thanks,
Conor