This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

General purpose isolated Led Driver ic?

Hello,

I have 3 types of isolated non-dimmable Constant Current Led Driver on design table with different input voltage ranges.
Output is similar to all these three types

Iout = 700 mA (Ioutripple 15 %) @ Uout = 10..32 V)

Input voltages:

a)    24/48 Vac    (19..55 Vac)    annual volume 2 kpcs
b)    115/230 Vac    (85..265 Vac)     annual volume 4 kpcs
c)    12 Vac    (9..16 Vac)    annual volume 0,5 kpcs

I think it is possible to do with one ic..?

Has TI something to offer for this design?

The type 'a' is most urgent case.

I appreciate any help you can give. 

Sincerely, Juha Koivisto