This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: TPS82130 0.2mm clearance on land pattern

Part Number: TPS82130


Tool/software:

I am using the Solder Mask Defined (SMD) land pattern of the TPS82130 MicroSIP package. This SMD land pattern is however not compliant with the board required clearance of 0,2mm.
Is it possible to either shrink the copper under the SMD land pattern by 0,025mm, or make it a NSMD land pattern by interchanging the copper and the solder mask opening?

Can you recommend an option?

  • Hi Sir,

    Usually we don't suggest change SMD land pattern. But if it is not compliant with the board required clearance , I think the first option you mentioned would be better, just make sure there is no electrical rule violation。

    Thanks

    Colin