This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064RNQEVM: Evaluation way with USB PD Controller TPS65987D

Part Number: TUSB1064RNQEVM
Other Parts Discussed in Thread: TUSB1064, TPS65982, , TPS65987D

Tool/software:

Dear Team,

My customer is considering  USB Type-C PD DisplayPort Alternate Mode application, and it is DP Alt-Mode Sink-Side. I have promote the TUSB1064 for Alt-Mode MUX and the TPS659687D for Alt-Mode USB PD Controller to them.
There is the TUSB1064RNQEVM, but USB PD Controllre on this EVM is TPS65983ACZQZR (from BOM) / TPS65982 (NRND) (from schmatic).

Are there any evaluation way of the TUSB1064RNQEVM with the TPS65987D EVM?

If there is a evaluation way, is there a project file of TPS65987D to control the TUSB1064 in I2C mode?

Best Regards,

Koshi Ninomiya

  • Hi Koshi,

    You can look at the TUSB564-Q1 EVM for a reference on using the TUSB1064 with the TPS65987D. The 564-Q1 has the same pinout as the 1064, so the connections should be the same. Note that the 564-Q1 pin numbers are different than the 1064:

    is there a project file of TPS65987D to control the TUSB1064 in I2C mode?

    We do not have a project file for this. I recommend reaching out to the PD controller team that supports the TPS65987D to see if they have one.

    Best,

    Shane