This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM70880-Q1: Current Capability Confirmation

Part Number: LM70880-Q1

Tool/software:

Hello Texas Instruments Team,

I would like to use the LM70880-Q1 to Convert a 48V Nominal(38V-76V Max) Input to 28V Output.

Can this Device Provide 8A?