Tool/software:
Hi E2E team,
Please help me review the schematic and HW setting for TPS25942A.
Condition:
Vin(normal)=12V
ILimit=1.18A
V(OV)=13.25V
V(UV)=10.85V
In addition, I have the following items that I would like to consult with TI:
[1] nFLT and PGOOD
I would like to connect these two signals to MCU. Due to power domain of MCU, I use the 1.8V for these two signals. is it ok?
[2] IMON
I'm not sure this signal can be directly connected to the ADC pin of the MCU. if that can be happen, The RIMON resistor value must be recalculated.
In this case, V(IMONmax) is 1.8V?
BR,
Caspar