Tool/software:
I want to create -2.5V from 5V. An output current of 20mA is sufficient.
If the current consumption is small, when calculating the standard inductor value, it comes out to a very large value of 130uH.
Would it be okay to use 4.7uH?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I want to create -2.5V from 5V. An output current of 20mA is sufficient.
If the current consumption is small, when calculating the standard inductor value, it comes out to a very large value of 130uH.
Would it be okay to use 4.7uH?

Hi Haruyasu,
It is ok to use 4.7uH.
BR
Patrick