This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630 Design - R,L,C components

Other Parts Discussed in Thread: BQ24630

Customer is looking to use  bq24630 battery charge IC as shown in Fig.1 on the datasheet SLUS894-January 2010.

     He wants to meet the following parameters:
     (LiFePO4 cells)

     1. Battery charging voltage: 14.6V .
     2. Charger input voltage:  16.75V to 18.0V .
     3. Input adapter current regulation:  4.0A .
     4. Battery charge current: (we have 2 different chargers)
         Charger A:  1.15A .
         Charger B:   0.75A .
    5.  Charge termination current:
         Charger A:  0.11A .
         Charger B:  0.075A .
   
     Question 1: Need Inductor, resistor, and capacitor values to satisfy above parameters.

    Question 2: Did not see a value for the max. current that STAT1 and STAT2 outputs can sink.
        5mA is shown as a test condition on the Vout_lo line on the datasheet, is this the max?

   Thanks...