This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R2: Discrepancy in current calibration during Learning Cycle with BQ27Z561

Part Number: BQ27Z561-R2
Other Parts Discussed in Thread: BQ27Z561, BQSTUDIO

Tool/software:

Hi,

I am currently implementing the learning cycle using the BQ27Z561 fuel gauge IC on an LP353035 LiPo battery (3.7V, 400mAh). However, I am encountering discrepancies in the current values during calibration.

For instance, when I discharge the battery and calibrate the current to -1A, the discharge proceeds correctly. But when I charge the battery the power supply device shows 181mA, while bqStudio reports 202mA.

Could you explain why this discrepancy occurs and suggest how to calibrate the system to ensure the current values on both the load device and bqStudio match accurately?

Thanks,

Ruchika