Tool/software:
We are trying to make our gate drivers go to ASC mode on reset by holding AI5 and AI6 at approximately 3.4V. In order to not trigger other safeties which are enabled on reset, we tried the following:
1. Pulling AI2 and AI4 to GND2 to not trigger OCP/SCP
2. Pulling VCECLP to GND2 to keep the voltage at that pin below the threshold
Additionally, CLAMP is left floating since we are not using the Active Miller Clamp.
When the gate driver powers on, it does not drive the gate on.
Based on the ASC Implementation Flowchart (Figure 7-27 in datasheet,) we weren't sure whether or not this would only work with VCC1 down, so we removed VCC1 with the above configuration and witnessed the same behavior.