Other Parts Discussed in Thread: TPS3808-EP
Tool/software:
Question #1
What is the suggested substitute part number from Texas Instruments for the Onsemi PN# NCV308SN500T1G?
Question #2
The TPS3808G01MDBVTEP is to Monitor a User-Defined Threshold Voltage.
The TPS3808G33MDBVREP is to monitor a 3.3 Threshold Voltage.
Can you provide information on the specifications and applications for PN# V62/08607-01XE, V62/08607-09XE that are listed in the TPS3808-EP ordering list?
Question #3
The absolute maximum RESET pin current is 5mA but what is the recommended maximum RESET pin sink current
Question #4
What value of pullup resistor is recommended for the RESET Line if the voltage on the open-drain RESET line is 5V?