Tool/software:
Hi, we are planning to make a battery eliminator circuits for UAVs with following specs:
Input voltage range 3S-12S lithium ion HV battery
Output voltages: 5.2V(compulsory), 7.5V(optional), 9V(optional), 12V (Optional, when input is at least 4S) at 3A max.
We chose to have a synchronous converter to achieve small solution size. Since the end use is in drones with high current BLDCs (40-120A continuous for all motors combined), the converter may see some input voltage transients. Is it recommended to still use LM76003 for the same? Or something with higher Vin pin AMR should be used (sync/non-sync)?