This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3803: we need to calculate the transformer turns ratio, which we are unable to do.

Part Number: UCC3803
Other Parts Discussed in Thread: UCC2897A

Tool/software:

Hi,

We are developing an isolated power supply circuit using the UCC3803.

We have set the switching output of the FET (IRFR120NTRPBF) to 12V, and the transformer's input is 24V.

We want an isolated output of ±100V. Based on these parameters, we need to calculate the transformer turns ratio, which we are unable to do. I am providing reference.

If anyone has a reference design, please provide it.