This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: LED open circuit fault, one of the conditions {V(SUPPLY) > V(ADCLOWSUPTH)}, V(ADCLOWSUPTH) value setting problem.

Part Number: TPS929120-Q1


Tool/software:

TPS929120-Q1 Operating voltage V(SUPPLY) 7.5V power supply, and V(ADCLOWSUPTH) register set 7V; The condition V(SUPPLY) > V(ADCLOWSUPTH) is valid, but the open circuit fault cannot be read; V(ADCLOWSUPTH) register value set 5V, 6V can read open circuit faults. May I ask the V(ADCLOWSUPTH) register value set 7V, the condition is true can not read the open circuit fault cause?

  • Can you measure SUPPLY pin and OUTx PIN VOLTAGE when opens and read status registers content? thanks. 

  • I can measure.

  • SUPPLY pin for 7.28v,V(ADCLOWSUPTH) register set 7V,fault pin voltage equals SUPPLY pin, faulty pin cannot read open circuit fault. what is the reason?

  • Can you help check if FLAG_ADCLOWSUP is set to 1? 

    The TPS929120-Q1 uses its internal ADC to monitor supply voltage V(SUPPLY). TPS929120 ADC is 8 bit and it's not very high resolution, INL is +/2LSB, which is +/- 0.16V for SUPPLY voltage.

    In this case, SUPPLY & V(ADCLOWSUPPTH) are too close. If there is ripple/noise or dynamic response, it is possible to trig ADCLOWSUP. 

    The LED open-circuit and single LED short circuit detection is disabled if the supply voltage is below threshold to avoid LED open circuit and to prevent the single LED short-circuit fault from being mis-triggered. Refer to Programmable Low Supply Warning in datasheet 

    You may either increase input voltage or set lower V(ADCLOWSUPTH)