This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: BQ24650 Battery Charger

Part Number: BQ24650

Tool/software:

Dear Team,

Good day,
I am reaching out regarding the BQ24650 battery charger. I understand that this component is designed for charging purposes. Could you please confirm whether an additional discharge control circuit is required for managing the discharge process of the battery?
Regards,
Amith N
  • Hello Amith,

    No, you should not need an additional discharge control circuit.

    Best Regards,

    Christian

  • HI,

    Thank you for the confirmation. Please verify if the highlighted path in red is for battery discharging is correct. Additionally, we seek clarification on how the load receives power during charging. Is the power supplied through the path highlighted in green?

    Our current understanding is that the load will be powered directly from the input source, with the input being distributed between charging the battery and supplying the system load. Please confirm whether this assumption is accurate.

  • Hello Amith,

    Please verify if the highlighted path in red is for battery discharging is correct. Additionally, we seek clarification on how the load receives power during charging. Is the power supplied through the path highlighted in green?

    Yes, This is correct.

    Our current understanding is that the load will be powered directly from the input source, with the input being distributed between charging the battery and supplying the system load. Please confirm whether this assumption is accurate.

    Yes, This is correct.

    Best Regards,

    Christian.

  • Dear Team,

    Im using 6.4V LiFePo4 battery so i need to consider VBAT voltage is 6.4V or less or more (if less how much less, if more how much more), and how can i set charging voltage and discharging voltage thresholds.

  • SHello Amith,

    I'm confused on your question. 

    Here is the BQ24650 schematic checklist: BQ24610_BQ24650_Schematic_Checklist (44).pdf

    In this checklist we have different calculations for the charge voltage, battery recharge threshold, and the battery low voltage threshold.

    Best Regards,

    Christian.