Other Parts Discussed in Thread: TIDA-01405,
Tool/software:
Hello,
I want to generate the -1.8V@1A-2A from 3.3V to 5.5V input voltages.
I have go through the TIDA-01405 and the refernce design and it is prefectly suitable for my requirement but I cannot find any EVM to test.
Que1 :- How can I found the EVM for this design?
Que2 :- Should I use the reference design schematic in my design to generate the -1.8V?
I have got the TPS82130EVM-720 but this design is to genertae the +1.8V.
Que3 :- Can I use the TPS82130EVM-720 to genertare the -1.8V?
Regards,
Alpesh