Other Parts Discussed in Thread: TPS7A03, , TINA-TI, TPS61040, TPS61096A
Tool/software:
Hi Texas Instruments Team,
I am currently working on a project involving a Geiger tube detector that requires an operational voltage of 400V with very low current consumption (less than 0.1mA). The available input voltage for this circuit is 3.3V, and I am seeking a solution to efficiently boost this to 400V DC with ultra-low power consumption.
I have designed a preliminary circuit using TINA-TI, incorporating the TPS7A03 LDO to boost the voltage from 3.3V to 5V. My plan involves using a low Rds(on) MOSFET in conjunction with the TPS61175 boost converter. However, I am not certain if this approach can meet my requirements. The circuit diagram is included below for your reference.
My primary concern is achieving the necessary 400V with minimal quiescent current and overall power consumption, as this circuit will be used in a portable, battery-powered radiation detector device. Ideally, the power consumption for boosting from 3.3V to 400V should be less than 500µA.
Alternatively, if it is feasible to boost the 3.3V to 100V, I could utilize a four-stage Cockcroft-Walton voltage multiplier to achieve the 400V. If boosting to 70V or higher is possible, a six-stage multiplier could also be considered.
I would appreciate any recommendations or insights you can provide regarding the feasibility of this approach and any alternative solutions or components that might better meet these requirements.
Thank you for your assistance.
Best regards,
Zaim