This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751: TPS25751 - Interrupt Event for I2C1 Interrupt Event for I2C1 register 14h

Part Number: TPS25751

Tool/software:

I'm writing driver for TPS25751 and I have notice that there is a issue in documentation for Interrupt Event for I2C1 Interrupt Event for I2C1 register [ID: 14h]. Where are typo in count of bits and there might be an issue when I'm asking for this during Pushing Bundle. 

I have received 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00001011 and I don't knew if field Ready for Patch was send to me or not 

b00001011 = dec:11