Other Parts Discussed in Thread: TPS62932
Tool/software:
Dear forum
I'm working in a solar panel regulator that has to reduce the solar panel voltage from 21V open circuit and 17.5V (MPP) to 15V
my idea is to use a DC/DC buck converter, but this converter has to bypass the input to the output
when the input voltage gets equal or less than the output voltage. (and to start switching again when vin > vout)
Can you suggest me a TI part/s with that characteristic? The current output needed is 2A max
Thanks in advance
Ignacio