This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61377EVM: Achieve 6A output current

Part Number: TPS61377EVM


Tool/software:

Hi team,

I want to use this EVM to achieve 6A output current, however, the default current is 1.5A. 

What changes do I need to make on this EVM? Change the inductor to meet the Isat?.

Vin: 12V-16.8V(4s3p)

Vout: 24V

Ioutmax: 6A.