This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

120W 230Vac @ 50Hz to 12Vdc @ 10A part recommendation

Part Number: UCC29910A
Other Parts Discussed in Thread: TPS546D24A, UCC29910A

Tool/software:

Dear TI team

I am gonna use TI Ic for Auxiliary power supply

suggest High efficiency,low cost control IC to do this

Requirement is 120W,12V,10A DC,input is 230 V ac 50HZ

kindly suggest control IC

i may plan to go through synchronous buck

Thank you

  •  

    Unfortunately, because you tagged your question with a medium voltage (18V Vin Max) non-isolated DC/DC Buck regulator, the TPS546D24A, which does not support an AC input or a 12V output, your question was sent to the wrong group for support.  I am going to try and redirect your post to the correct group for support.

    In the future, even if looking for a part recommendation, it will help you receive a faster response if you can find a part that at least works for your application first, and tag that part.

    My initial recommendation would be to consider a BUCK PFC such as theUCC29910A, which can produce a 12V output directly from a 230V input without first boosting it up, then stepping it down.

  •  

    I have made edits to your post and redirected it to our High Voltage product line who should be able to assist you.

  • Hello Venkatesh, 

    AC-powered applications > 75W usually (although not always) require power factor correction (PFC). 
    If this is true for your application, then UCC29910A is a possible 1-stage solution, as Peter suggested above. 
    Output capacitance can be extraordinarily large, however, depending on your hold-up and output ripple requirements.

    But if your application also need isolation from the AC line, then the UCC29910A alone is not sufficient; an isolating DC-DC stage will be necessary.
    Or, an isolating single-stage Flyback-PFC can be developed for 12V out, but again will require significantly large Cout. 

    For a 120-W power level I suggest using UCC28056C for the PFC controller, if you need PFC.
    For the DC-DC stage, I suggest using UCC28C50-series PWM controller as a flyback or forward mode converter.   

    Regards,
    Ulrich

  • Thank you so much

    i will check with design 

    Regards

    venkatesh B